Technical Forum

SIMODRIVE Converter system

communication S7 314 avec SIMODRIVE 611

Thread Starter: mayana   Started: 5/22/2012 10:55 PM   Replies: 2

« Previous thread Next thread »
Page 1 of 1 (3 items)
  5/22/2012, 10:55 PM
Joined 5/22/2012
Last visit: 6/4/2012
Posts: 2
Rating:
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
salut
je suis nouvelle sur le forum bon j'ai une question :
j'ai fait une migration s5 vers s7 bon sur l'encienne instalation il y a un simodrive 611 (alimentation + regulation ) es que  je peut faire une communication profibus DP slave avec l'automate S7-314 2PN -DP ?

comment avoir le simodrive sur le TIA portal j'ai pas trouvé sur  le catalogue ? Rnf:lblSmileyTooltip_

                                                                                                          Cordialement 
Top
  5/22/2012, 11:06 PM
Joined 9/27/2006
Last visit: 5/24/2013
Posts: 3949
Rating:
Rated: Excellent [4.15 out of 5 / rated 620 time(s)]. (620) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
mayana wrote:
salut
je suis nouvelle sur le forum bon j'ai une question :
j'ai fait une migration s5 vers s7 bon sur l'encienne instalation il y a un simodrive 611 (alimentation + regulation ) es que  je peut faire une communication profibus DP slave avec l'automate S7-314 2PN -DP ?

comment avoir le simodrive sur le TIA portal j'ai pas trouvé sur  le catalogue ? Rnf:lblSmileyTooltip_

                                                                                                          Cordialement 


Translation from the French:
mayana wrote:
Hello, I am new to the forum, and I have a question:
I have migrated a S5 system to S7; in the old configuration there is a simodrive 611 (power supply + regulation ). Can I setup a Profibus-DP slave communication with a S7-314 2PN -DP ?

Where can I find the Simodrive 611 on theTIA portal, I cannot locate it in the catalog ? 
                                                                                                          Cordially,





=== Edited by dchartier @ 5/22/2012 11:06 PM [GMT ] ===


Top
  5/22/2012, 11:13 PM
Joined 9/27/2006
Last visit: 5/24/2013
Posts: 3949
Rating:
Rated: Excellent [4.15 out of 5 / rated 620 time(s)]. (620) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Hello mayana;
The Siemens A&D forum is divided in 2 sections, one in German, the other in English. Please make an effort to use English in this section of the forum, as it is the language most users share here, even though it might not be their mother tongue.

As a first answer to your question on Simodrive 611 and Profibus-DP communications, please have a look at this older thread:
https://www.automation.siemens.com/WW/forum/guests/PostShow.aspx?HTTPS=REDIR&PostID=216246&language=en
Many members offer some good tips and links for more information on the same subject.

Hope this helps,
Daniel Chartier

As to your second question:
To see a new DP-slave in the Profibus catalog of any Profibus configurator, you need to add the gsd file (electronis data file) for that slave in the configuration software. See the online help of the TIA portal for more details.
Here is a quote from the following FAQ:
http://support.automation.siemens.com/WW/view/en/24210648

QUESTION:
The GSD file SIEM808F.GSD that is supplied with toolboxes - software releases 09.02., 10.01. and 10.02. - cannot be downloaded.

ANSWER:
However, the GSD file with the same name can be used from toolboxes of earlier software releases.


Here is a Downloads page from Siemens Support where you can find different downloads for the Simodrive 611U sotware releases (they include each a gsd file) based on version:
http://support.automation.siemens.com/WW/view/en/10804911/133100
D.C.



=== Edited by dchartier @ 5/23/2012 1:00 AM [GMT ] ===


=== Edited by dchartier @ 5/23/2012 12:54 AM [GMT ] ===
Added link to Simodrive 611U packages

Top
Page 1 of 1 (3 items)
Actions