Technical Forum

STEP 7 Additional Software

PLCSIM 5.4 with Windows 7

Thread Starter: porsche00   Started: 5/15/2012 12:55 PM   Replies: 3

« Previous thread Next thread »
Page 1 of 1 (4 items)
  5/15/2012, 12:55 PM
Joined 5/15/2012
Last visit: 6/9/2012
Posts: 1
Rating:
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
hi:  
can you give me :" HKEY_LOCAL_MACHINE\SOFTWARE\Siemens\AUTSW\PLCSim  "
i want to  install PLCSIM V5.4 SP4 on Windows 7  
thanks  
----------------------------------form a 
Chinese friend



=== Bearbeitet von Blue Moderator @ 15.05.2012 13:10 [GMT ] ===
splitted and renamed from PLCSIM 5.4 unter Windows 7 installieren

=== Bearbeitet von porsche00 @ 15.05.2012 13:04 [GMT ] ===


=== Bearbeitet von porsche00 @ 15.05.2012 13:03 [GMT ] ===


Top
  5/15/2012, 3:20 PM
Joined 10/10/2005
Last visit: 5/17/2013
Posts: 796
Rating:
Rated: Outstanding [3.37 out of 5 / rated 27 time(s)]. (27) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 

Hello,

you need the SP5 and Upd1 for your S7-PLCSIM V5.4 or install STEP 7 Professional 2010 which included S7-PLCSIM and is compatible for Windows 7.

See also the informations under the following link:

http://support.automation.siemens.com/WW/view/de/51884395

With best regards
Cicero

Top
  5/18/2012, 7:38 PM
Joined 7/25/2009
Last visit: 5/18/2013
Posts: 398
Rating:
Rated: Very Good [1.5 out of 5 / rated 4 time(s)]. (4) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Cicero wrote:

Hello,

you need the SP5 and Upd1 for your S7-PLCSIM V5.4 or install STEP 7 Professional 2010 which included S7-PLCSIM and is compatible for Windows 7.

See also the informations under the following link:

http://support.automation.siemens.com/WW/view/de/51884395

With best regards
Cicero



Hi ciero
its working in os widows 7 once agin i restarted and downloaded the hardwre in step7 400 module hanging more and more and stuck up why in widows vista OS...?

regards
algudkar

regards
Algudkar sh..

Top
  5/18/2012, 7:53 PM
Joined 3/21/2006
Last visit: 5/14/2013
Posts: 9063
Rating:
Rated: Outstanding [3.78 out of 5 / rated 820 time(s)]. (820) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
On Monday check your messages.

Best regards,
Hristo Mihalev
Top
Page 1 of 1 (4 items)
Actions