Technical Forum

SIMATIC ProTool / ProTool/Pro

Windows Vista

Thread Starter: dande74   Started: 3/15/2010 4:53 PM   Replies: 3

« Previous thread Next thread »
Page 1 of 1 (4 items)
  3/15/2010, 4:53 PM
Joined 2/5/2007
Last visit: 5/28/2013
Posts: 96
Rating:
Rated: Above avarage [2.33 out of 5 / rated 3 time(s)]. (3) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Hi!

I know that ProTool isn't compatible with Vista. Just wondering if anyone have tried to install an run it.

1. Will it install?
2. Can you strat the app?
3. Can you edit project?
4. Can you download to a panel?

I mean, sometimes programs not compatible works enough for small amount of work.

Regard

    -- Daniel
Top
  3/17/2010, 10:06 PM
Joined 2/5/2007
Last visit: 5/28/2013
Posts: 96
Rating:
Rated: Above avarage [2.33 out of 5 / rated 3 time(s)]. (3) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
dande74 wrote:

1. Will it install?


No, it's not possible to install. Ended up with OS not supported...
Top
  5/6/2012, 10:05 PM
Joined 7/3/2006
Last visit: 5/19/2013
Posts: 51
Rating:
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 

 

Dear friend

to do so first make a copy of your CD on your H.D

search all file of protool cd for *.exe files and open the properties for every file

Through the compatibility of each file choose windows xp sp2 or sp3 for each exe file

after finishing for all files now try to install the software , I tried this and it is OK

 

Best regards

Top
  5/7/2012, 1:58 PM
Joined 9/5/2011
Last visit: 6/19/2013
Posts: 2736
Rating:
Rated: Outstanding [3.8 out of 5 / rated 136 time(s)]. (136) 
Users with special expertise supervising conferences
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Hello,

You can see which operating system do you can use with ProTool in the following FAQ.

Which versions of SIMATIC ProTool/Lite, SIMATIC ProTool and SIMATIC ProTool/Pro are compatible with which Windows operating systems?

Tweety
Top
Page 1 of 1 (4 items)
Actions