Technical Forum

SIMATIC TDC, FM458, T400

Limitation using message block in TDC

Thread Starter: Aniketdas   Started: 5/4/2012 3:27 PM   Replies: 5

« Previous thread Next thread »
Page 1 of 1 (6 items)
  5/4/2012, 3:27 PM
Joined 12/7/2011
Last visit: 3/22/2013
Posts: 16
Rating:
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 

Hi Eveyone...

In TDC do we have any limitations in inserting message block "MSG"?If there is any limitation then how many block we can use per TDC CPU.

Regards,
Aniket
Top
  5/4/2012, 4:15 PM
Joined 8/25/2006
Last visit: 5/22/2013
Posts: 899
Rating:
Rated: Excellent [4.2 out of 5 / rated 85 time(s)]. (85) 
Users with special expertise supervising conferences
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Hello.
If you mean function blocks @MSC, MERx and MSIx, then the only limitation is one @MSC block per CPU.
Top
  5/4/2012, 4:16 PM
Joined 8/31/2005
Last visit: 5/22/2013
Posts: 981
Rating:
Rated: Outstanding [3.85 out of 5 / rated 122 time(s)]. (122) 
Users with special expertise supervising conferences
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
You can use one @MSC block per CPU.

I did not found a MSG block in the documentation. If it is not missspelled, it may be a user function block. Ín this case you have to ask the developer of the the user function block libary.

mfG / Best Regards

Dirk
Top
  5/7/2012, 1:16 PM
Joined 4/27/2012
Last visit: 5/23/2012
Posts: 22
Rating:
Rated: Very Good [2 out of 5 / rated 3 time(s)]. (3) 
This might help..
www.automation.siemens.com/mcms/industrial...tdc/.../Default.aspx
Top
  5/7/2012, 2:09 PM
Joined 8/25/2006
Last visit: 5/22/2013
Posts: 899
Rating:
Rated: Excellent [4.2 out of 5 / rated 85 time(s)]. (85) 
Users with special expertise supervising conferences
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Aniket S Dange wrote:
This might help..
www.automation.siemens.com/mcms/industrial...tdc/.../Default.aspx

Hello.
Link is not complete.
Top
  5/24/2012, 7:10 AM
Joined 5/21/2012
Last visit: 5/26/2012
Posts: 6
Rating:
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 

we have simatic tdc with cpu 551..in one cpu ,we are using about 400 'msg' blocks, stil its all are working..so i think not any limitation for insert 'MSG' block in cfc for TDC...

Top
Page 1 of 1 (6 items)
Actions