Technical Forum

Process Instrumentation / Analytics / Weighing Systems SIWAREX

ultramat 23 analog output problem

Thread Starter: islam elamrawy   Started: 4/28/2012 12:22 PM   Replies: 2

« Previous thread Next thread »
Page 1 of 1 (3 items)
  4/28/2012, 12:22 PM
Joined 4/28/2012
Last visit: 5/2/2012
Posts: 7
Rating:
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
I have a problem with Ultramat 23 analyzer. The analog output of the analyzer is connected to PCS7 system via analog input cards SM331. All four analog readings are ok in analyzer but it gives bad quality error (for second then return ok again)in pcs7 system while the reading are ok (no open loop values).I made test for the analog output of analyzer from its menu and measured with multi-meter and values are ok. Can you help me with this problem?
Regards
Top
  4/28/2012, 12:48 PM
Joined 3/18/2008
Last visit: 5/9/2013
Posts: 256
Rating:
Rated: Outstanding [3.86 out of 5 / rated 44 time(s)]. (44) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Dear islam elamrawy,
which type of analog input you are using?
Is it voltage or current? & Which Analog input module you are using?
Please provide the MLFB for the same.


THANKS & REGARDS,

Solution is always available for all Problems.
The thing is to Work hard On it.
I Hope this is the best solution for your problem.
Please Give Feed back if you are happy with My Answer.
Top
  4/28/2012, 2:46 PM
Joined 4/28/2012
Last visit: 5/2/2012
Posts: 7
Rating:
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 

I use current 4-20 mA four wires. The reading was ok before but suddenly the problem occurred

Top
Page 1 of 1 (3 items)
Actions