Technical Forum

Visualization

WINCC or WINCC flexible--MODBUS

Thread Starter: m.aksoy   Started: 3/18/2012 9:19 AM   Replies: 1

« Previous thread Next thread »
Page 1 of 1 (2 items)
  3/18/2012, 9:19 AM
Joined 3/16/2012
Last visit: 5/19/2013
Posts: 11
Rating:
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
hi friends.

I want to make an application.

My system is consists of Carel PCO controller (2 pieces), Hvac unit (2 pieces).
The communication protocol of these unit MODBUS.

I want to monitor and control them with wincc or wincc flexible.
Is it possible for such a thing?
How I can be done if something like that.

How can I convert Modbus tags to Wincc/Wincc flexible tags? 

I need your help,
best regards.

Top
  3/20/2012, 12:44 PM
Joined 4/24/2009
Last visit: 5/19/2013
Posts: 1948
Rating:
Rated: Outstanding [3.89 out of 5 / rated 100 time(s)]. (100) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Thread closed, because question is already published in the following thread flexible modbus

Best regards
O_Moderator
Top
Page 1 of 1 (2 items)
Actions