Technical Forum

Other Process Control Systems

BRAUMAT 6.0;Call of DFM (Type :1) in sequence FB

Thread Starter: Ner   Started: 3/14/2012 5:50 AM   Replies: 0

« Previous thread Next thread »
Page 1 of 1 (1 items)
  3/14/2012, 5:50 AM
Joined 2/23/2010
Last visit: 3/20/2013
Posts: 14
Rating:
Rated: Excellent [5 out of 5 / rated 1 time(s)]. (1) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Dear expert,
I am working on BRAUMAT 6.0, using DFM group 2, DFM2.11, as type 1:timer.
This DFM is already called in Sequence 5 FB1006, I need to use this DFM in Sequence 12,FB1012 again.
DFM 2.11 is called in FB1006.
These sequences never,never run together.
The timer release bit is used in correct way as it must be.
But when I am Using DFM2.11 in sequence 12, it does not work, it works only when it is called the second time the FB1012 as well.
It seems that the other type DFMs say TYPE 4, the DFM can be called only once in any sequence FB and it works correctly, but the timer type DFM needs to be called in each sequence FB, no matter how many times.
The question is why do we need to pass on parameters to the DFM FC twice?
Want to know how the time slices affect this functionality - if at all !
Top
Page 1 of 1 (1 items)
Actions