Technical Forum

Process Control System - QUADLOG

process suite (4-mation) upgrade

Thread Starter: Pioneer   Started: 10/13/2009 11:12 AM   Replies: 1

« Previous thread Next thread »
Page 1 of 1 (2 items)
  10/13/2009, 11:12 AM
Joined 9/18/2008
Last visit: 5/18/2013
Posts: 51
Rating:
Rated: Very Good [2 out of 5 / rated 2 time(s)]. (2) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
dear all

we are using MOORE-QUADLOG system with operator station which is connect to the PLC by MNET and the engineering software is process suite(4MATION) and the supervision software is FastTools  with base of Windows NT OS.

now we want to upgrade the system as we want to use Windows XP for our stations.

please I have spme questions:

 

  • what is the new version of process suite (running on Windows XP)?
as  it is mentined in some forumes there is new solution by PCS7 :

 

 

  • there is two softwares, wich of them must be used,SIMATIC PCS 7 APACS+ OS or APACS Control 7.0 ?what is diffrences?
  • which software will be use as engineering?
  • which software will be used as supervision?
please help me as we need to upgrade the system urgently.

 

thanks in advance.




=== Edited by Pioneer @ 10/13/2009 12:30 PM [GMT ] ===



Pioneer
Top
  3/24/2010, 9:01 PM
Joined 1/26/2010
Last visit: 4/19/2013
Posts: 4
Rating:
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 

Hi Pionner,

I understand that:
  • The new version of process suite (running on Windows XP) is PCS7 (WinCC).
  • The "SIMATIC PCS 7 APACS + OS" is the whole package HMI migration only, while "APACS Control 7.0" is just a part of package, this part is a software installer "4-mation" because when making the migration of HMI, will need the "4 -mation "(XP compatible) for the configuration of the APACS / QUADLOG controller.
  • If migrate HMI only, the engineering software to use is the "4 mation" and the DBA.
  • The software supervision is PCS7.

Best Regards,
Amanuel.
Top
Thank you for this post from:
Page 1 of 1 (2 items)
Actions