Contact
Home
|
Product Support
|
Applications & Tools
|
Services
|
Forum
|
mySupport
Login
|
Register
Print document
Technical Forum
Communication / Networks
Modbus General Description
Thread Starter:
smiffy
Started:
12/15/2011 6:41 PM
Replies:
25
Next thread »
«
‹
1
2
3
›
»
Page 2 of 3 (26 items)
5/6/2012, 1:08 PM
gre_m
Joined 9/27/2005
Last visit: 6/17/2013
Posts: 944
Rating:
(36)
(0)
modbus exist on rs422/485/232 as add on over ptp-communication and add-on over ethernet/TCP=modbus TCP. Profibus - is
all-sufficient prtocol, therefore modbus as add-on over profibus not exist.
Top
5/6/2012, 2:05 PM
smiffy
Joined 1/17/2007
Last visit: 6/19/2013
Posts: 766
Rating:
(143)
(0)
I think they were hinting that I could do a similar document to explain the basics of Ethernet and Profibus (and maybe even Profinet). I don't think that they were suggesting that modbus can be setup over a Profibus interface.
I will see what I can do to come up with Ethernet and Profibus documents. However, these things tend to take quite a bit of effort and time. I will also need some proof reading services from my fellow experts.
Programming today is the race between software engineers building bigger and better idiot proof programs, and the universe producing bigger and better idiots.
So far, the universe is winning...
Top
5/6/2012, 4:02 PM
Arunraje
Joined 4/4/2012
Last visit: 5/18/2013
Posts: 75
Rating:
(9)
(1)
Ya Smiffy please do the needful...
Regards.
"Nothing is permanent, except the CHANGE"
Top
5/6/2012, 8:08 PM
AUTOMATION_BOUHA
Joined 5/5/2012
Last visit: 10/9/2012
Posts: 2
Rating:
(0)
(0)
Thank u SMIFFY thats nice from u, that will help us more, and i hope that we don't bother u
Top
5/7/2012, 1:11 PM
Aniket S Dange
Joined 4/27/2012
Last visit: 5/23/2012
Posts: 22
Rating:
(3)
(0)
Dear Arun,
this will surely help you..
http://www.plcmanual.com/isoosi-model
Enjoy..
Top
Thank you for this post from:
Arunraje
7/20/2012, 4:00 AM
YvonV
Joined 6/6/2012
Last visit: 12/19/2012
Posts: 24
Rating:
(0)
(0)
its a good read. thank you for that effort.
Yvon
Top
Thank you for this post from:
sorooshi
,
smiffy
9/29/2012, 9:21 AM
Hunky
Joined 10/7/2006
Last visit: 6/4/2013
Posts: 79
Rating:
(5)
(0)
Thank you for the support.
I am a little confused here.
I am doing a project where in i have to communicate with ABB DCS with CP 441-2. The following is the requirement.
Data from DCS to PLC
Analog Output - Address : 400001
Digital Output - Address : 00001
Data from PLC to DCS
Analog Input - Address: 300001
Digital Input - Address :100002
In the above circumtances,CP 441-2 shoule be acting as Slave / Master?
If it is acting as a Slave will it read the data from DCS.
Thanks for your support and co-operation.
BR
MIA
Top
9/29/2012, 12:37 PM
Kaulquappe
Joined 11/27/2007
Last visit: 6/18/2013
Posts: 877
Rating:
(61)
(0)
Hello Hunky,
the used addresses do not imply any information which communication partner is master and which one is slave. It depends on the application on site. The master is the active one, it can read data from and write data to the slave. The slave can't initiate communication, it can just answer the client's requests.
You have just to ask whether the DCS acts as master or not.
Regards,
Kaulquappe
Top
Thank you for this post from:
dchartier
9/29/2012, 12:42 PM
dchartier
Joined 9/27/2006
Last visit: 6/19/2013
Posts: 4032
Rating:
(622)
(0)
Hunky wrote:
Data from DCS to PLC
Analog Output - Address : 400001
Digital Output - Address : 00001
Data from PLC to DCS
Analog Input - Address: 300001
Digital Input - Address :100002
In the above circumtances,CP 441-2 shoule be acting as Slave / Master?
Hello hunky;
It is indifferent which of the 2 (CP 441-2 or DCS) is master on the bus, especially if you have only these 2 nodes on Modbus RTU.
Choose one to be master based on ease of programming and familiarity,
If you select the DCS as master, you will have to program the Modbus jobs in the DCS, and choose:
- Write multiple coils (Modbus function 15- write to the 0000x outputs of the PLC)
-Write multiple registers (Modbus function 16- write multiple 4000x registers to the PLC)
-Read input registers (Modbus function 04- request 3000x registers from the PLC)
-Read discrete insputs (Modbus function 02- request 1000x inputs from the PLC)
Of course if the roles are reversed you would have to select the Modbus jobs in the Cp 441-2 so you would write digital and analog inputs to the DCS, and read digital and analog outputs to the PLC.
The slave will only reply to the master when Modbus jobs are sent to it, so everything is to be planned from the master's point of view.
I do not know how difficult it is to use Modbus RTU on your DCS, but it might be easier to let the CP 441-2 act as a slave, there would very little programming to be done on that side. Have a look at the following sample program for Modbus slave functions proposed by member Amit recently:
https://www.automation.siemens.com/WW/forum/guests/PostShow.aspx?HTTPS=REDIR&PostID=359580&language=en
Hope this helps,
Daniel Chartier
=== Edited by dchartier @ 9/30/2012 5:22 PM [GMT ] ===
Top
10/3/2012, 12:16 PM
Saggy
Joined 11/8/2011
Last visit: 6/10/2013
Posts: 183
Rating:
(33)
(0)
Thank you its very useful,I hope that you can explain to us more about profibus and ethernet protocols
Top
«
‹
1
2
3
›
»
Page 2 of 3 (26 items)
Actions
Copy Link
To conference
Product Conferences
LOGO!
SIMATIC TDC, FM458, T400
SIMATIC S7 - Hardware
SIMATIC S5 / STEP 5
SIMATIC 505
Communication / Networks
Programming Devices
PC-based Automation
Industrial PC SIMATIC PC
Decentral Peripherie
Industrial Software
SIMATIC Addons / IT4Industry
Process Control Systems SIMATIC PCS 7
Teleperm M / WinCC-TM / PCS 7 - TM
Process Control System - APACS+
Process Control System - QUADLOG
Other Process Control Systems
Visualization
SINUMERIK / SIMODRIVES / MASTERDRIVES / SIMOTION / SINAMICS
SINUMERIK CNC automation systems
SIMODRIVE Converter system
SIMOVERT MASTERDRIVES
Motion Control System SIMOTION
SINAMICS
MICROMASTER
ROBICON Perfect Harmony - Medium voltage converters
DC converters SIMOREG
SIMOTICS
Drive Tools
Process Instrumentation / Analytics / Weighing Systems SIWAREX
SIMATIC Ident
Low-Voltage Controls
Building Technology
General Conferences
Quick Links
All Conferences
The new Threads
Highlight Threads
Contact
Support Request
Contacts Worldwide
Moderator
Users online
orosz
,
Pitti
,
T_Moderator
,
CS Moderator
,
granukirsche
,
857022
,
Jerommeke
,
RFD
,
azu
,
Günni
,
Tom40
,
dchartier
,
siohm
,
Der Tim
,
Sweet Lemonade
,
KSN
,
playerslight
,
Para-noja
,
carmamezo
,
SCADA-Engineer
Help
Online Help
Guided Tour