Contact
Home
|
Product Support
|
Applications & Tools
|
Services
|
Forum
|
mySupport
Login
|
Register
Print document
Technical Forum
MICROMASTER
Parameter adjustments to overcome high starting torque of pump motor
Thread Starter:
Shane Byars
Started:
7/20/2012 1:48 PM
Replies:
2
« Previous thread
Next thread »
Page 1 of 1 (3 items)
7/20/2012, 1:48 PM
Shane Byars
Joined 7/17/2012
Last visit: 2/4/2013
Posts: 1
Rating:
(0)
(0)
We are attempting to use a MM440 to drive a PD lobe pump. This pump has a characteristic high starting torque as compared to a centrifugal. When starting the pump motor the output shaft cogs and does not make one complete revolution. We then performed a "Motor Identification" via Starter and noted changes in Parameters 350 and 352 after the routine. We then modified P320 from 0 to 50, P346 from 0.117 to 1.0 and P1312 from 0 to 150. After doing this the motor would turn the pump. The parameter adjustments were suggestions from a Siemens tech support rep. What precisely is the proper way to commision a MM440 for operation with a high torque starting load? We have reviewed section 6 of the MM440 guide and followed these procedures. The motor is
2HP/2.5A rated inverter duty. Using a Fluke clamp ammeter we see an output of around 2.6A. The AOP indicates an output of 2A. What exactly is the "Magnetization current"?
Top
7/20/2012, 2:06 PM
Marcjan
Joined 4/22/2010
Last visit: 5/24/2013
Posts: 3213
Rating:
(295)
(0)
Shane Byars wrote:
What exactly is the "Magnetization current"?
That is the
No Load
current measured by the drive in autotune mode.
Regards,
Marcjan
Problem solved?
Please let us know!
Please no technical questions by PM, use the forum!
Top
8/14/2012, 9:19 AM
sparten
Joined 8/2/2011
Last visit: 5/21/2013
Posts: 96
Rating:
(4)
(0)
what is value of parameter p1300??????if possible then for pump app. make it p1300=2.....then after your problem not solve thrn try to run drive in SLVC mode p1300=20 make speed optimization p1960=1.........
Top
Page 1 of 1 (3 items)
Actions
Copy Link
To conference
Product Conferences
LOGO!
SIMATIC TDC, FM458, T400
SIMATIC S7
SIMATIC S5 / STEP 5
SIMATIC 505
Communication / Networks
Programming Devices
PC-based Automation
Industrial PC SIMATIC PC
Decentral Peripherie
Industrial Software
SIMATIC Addons / IT4Industry
Process Control Systems SIMATIC PCS 7
Process Control System - APACS+
Process Control System - QUADLOG
Teleperm M / WinCC-TM / PCS 7 - TM
Other Process Control Systems
Visualization
SINUMERIK / SIMODRIVES / MASTERDRIVES / SIMOTION / SINAMICS
SINUMERIK CNC automation systems
SIMODRIVE Converter system
SIMOVERT MASTERDRIVES
Motion Control System SIMOTION
SINAMICS
MICROMASTER
ROBICON Perfect Harmony - Medium voltage converters
DC converters SIMOREG
SIMOTICS
Drive Tools
Process Instrumentation / Analytics / Weighing Systems SIWAREX
SIMATIC Ident
Low-Voltage Controls
Building Technology
General Conferences
Quick Links
All Conferences
The new Threads
Highlight Threads
Contact
Support Request
Contacts Worldwide
Moderator
Users online
motmonti
,
MatijaZigic
,
Ashish Dixit
,
Axel_Wall
,
Kaoma MM
,
Ahmed Said AboEl-Kheir
,
andyoldenburg
Help
Online Help
Guided Tour