Hi, I have a problem with my S7-1200 (1214C DC/DC/DC). I tried to make a fast PWM work, but in some random time (after a weekend when noone touched PLC) I have an 24V always on my output Q0.0. It is very strange, because it is only on this output.
I checked it with my multimeter, and it was buzzing when I toutched Q0.0 and 3L (+24V). It has an resistance about 6Ohm.
Why such situation is happen? Please help.
If you connect an o-scope to the Q0.0 output does it look like a stable 24V or is it actually doing the PWM and the multimeter is simply too slow to react?
What control do you have on the PWM? 100%, 0%, 50%? Maybe a screenshot of the control logic could help.
Helpful? Rate it.
Solved? Post it.