Unless you have purchased two identical S7-400H CPU's, not standard CPU's there is no way you can have redundancy. I would allways advice to purchase a redundant bundle as these have been system tested for redudancy operation. Furthermore the S7-414-2DP as far as I remember is a standard CPU with 2 profibus DP ports with a fair number of years on its belt as currently there is no CPU with this name available (The current redundant version is 414-5HPN/DP and the current standard CPU versions are 414-2, 414-3, 414-3 PN/DP and 414F-3 PN/DP).
The IM151 redundancy bundle you reference is probably an IM151-8 which allows installation of a PROFINET (not PROFIBUS) in a redundant ring configuration between two H CPU's with firmware 6.0 as a minimum (brand new).
So I fear you are on the wrong track.
Following link provides you with the manual for redundant systems, I would suggest you read it first before attempting to waste a lot of time and money
https://support.automation.siemens.com/WW/llisapi.dll?func=cslib.csinfo&nodeid0=10805404&lang=en&siteid=csius&aktprim=0&extranet=standard&viewreg=WW&objid=10805188&treeLang=en
Kind regards,
David