Technical Forum

Motion Control System SIMOTION

Gain factor from WinCC Flexible

Thread Starter: Ivan_L   Started: 7/9/2012 5:43 AM   Replies: 8

« Previous thread Next thread »
Page 1 of 1 (9 items)
  7/9/2012, 5:43 AM
Joined 3/6/2012
Last visit: 2/12/2013
Posts: 10
Rating:
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
How to change the gain factor from the Flexible?  Can not write to the parameter _to.NameofAxis.TypeOfAxis.NumberOfDataSets.DataSet_1.ControllerStruct.PV_Controller.kv
Top
  7/9/2012, 6:44 AM
Joined 5/12/2006
Last visit: 5/23/2013
Posts: 1550
Rating:
Rated: Excellent [4.18 out of 5 / rated 115 time(s)]. (115) 
Users with special expertise supervising conferences
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Hello,

which error message ocurrs in WinnCCflex when you write the variable?
An which SIMOTION/WinCCflex version do you use`?


Regards
Christoph
Top
  7/9/2012, 8:51 AM
Joined 3/6/2012
Last visit: 2/12/2013
Posts: 10
Rating:
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
SIMOTION C240 v4.2, Scout 4.2 , WinCCFlex 2008 SP2
This parameter is not listed in the Flex. Where to find it?
Top
  7/9/2012, 11:57 AM
Joined 4/24/2006
Last visit: 5/22/2013
Posts: 4676
Rating:
Rated: Excellent [4.12 out of 5 / rated 428 time(s)]. (428) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Hello Ivan_L,

Perhaps it is a Compatibility problem. See the following link:
With what are SIMATIC WinCC flexible 2008, 2007, 2005 and 2004 compatible?

Best regards,

Wizard
Top
  7/14/2012, 10:45 AM
Joined 8/4/2010
Last visit: 5/16/2013
Posts: 117
Rating:
Rated: Excellent [5 out of 5 / rated 2 time(s)]. (2) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
SIMOTION C240 v4.2, Scout 4.2 , WinCCFlex 2008 SP2
i think they are compatible version
how can  i find mechanical parameter in flexible_?

J.SANCHEZ
Top
  7/14/2012, 3:38 PM
Joined 9/23/2005
Last visit: 5/13/2013
Posts: 286
Rating:
Rated: Outstanding [3.53 out of 5 / rated 17 time(s)]. (17) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Because thers's no such a parameter.
_to.name_of_axis.activeconfigdata.TypeOfAxis.NumberOfDataSets.DataSet_1.ControllerStruct.PV_Controller.kv
or
_to.name_of_axis.setconfig.TypeOfAxis.NumberOfDataSets.DataSet_1.ControllerStruct.PV_Controller.kv
Top
Thank you for this post from:
  7/16/2012, 5:38 AM
Joined 3/6/2012
Last visit: 2/12/2013
Posts: 10
Rating:
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
jacek d, you were right. Thanks!
Top
  7/16/2012, 8:05 AM
Joined 5/12/2006
Last visit: 5/23/2013
Posts: 1550
Rating:
Rated: Excellent [4.18 out of 5 / rated 115 time(s)]. (115) 
Users with special expertise supervising conferences
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
When you access the axis variables vie WinCC you can't use Setconfigdata/activeconfigdata.
This access is only for use in programms on the CPU.

Regards
Christoph
Top
  7/16/2012, 11:27 AM
Joined 3/6/2012
Last visit: 2/12/2013
Posts: 10
Rating:
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
_to.name_of_axis.setconfig.TypeOfAxis.NumberOfDataSets.DataSet_1.ControllerStruct.PV_Controller.kv := HMI_variable;

 In HMI_variable write from WinCCflex. 
Top
Page 1 of 1 (9 items)
Actions