Technical Forum

SIMOTICS

spindle motor 1PH7163-2ND23-0BC0

Thread Starter: Zlatkodo   Started: 6/29/2012 7:47 AM   Replies: 2

« Previous thread Next thread »
Page 1 of 1 (3 items)
  6/29/2012, 7:47 AM
Joined 6/29/2012
Last visit: 7/3/2012
Posts: 4
Rating:
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Siemens spindle motor 1PH7163-2ND23-0BC0
We need to rewind this motor (probably is 22 kW, 4 pole winding) but we have only empty stator core with no nameplate  or winding data .
Motor run trough the controller SIMODRIVE 611 , ( 0 to 1400 Hz at pulse frequency 3.2kHz).
We need help with all  nameplate  data especially : rated frequency and voltage, connection and duty cycle ( for example: 400 V,  50 Hz, Y, S1).
BTW, the best help would be to obtain  all the winding data, if possible.
Thanks in advance.
Zlatkodo
opetja@ymail.com

Attachment: DSCF3004.JPG  (9 Downloads)



=== Edited by Zlatkodo @ 6/29/2012 7:49 AM [GMT ] ===



Top
  7/3/2012, 1:29 PM
Joined 10/11/2006
Last visit: 6/19/2013
Posts: 813
Rating:
Rated: Outstanding [3.94 out of 5 / rated 88 time(s)]. (88) 
Users with special expertise supervising conferences
Rated: Above avarage [3 out of 5 / rated 1 time(s)]. (1) 
Hello,

I think it's not too easy to rewind such a motor Rnf:lblSmileyTooltip_  think

Attached a figure of the motor parameters.

Good luck blink

Attachment: 1PH7163-xxD.jpg  (10 Downloads)

Best regards
TechTeam

Top
  7/3/2012, 6:59 PM
Joined 6/29/2012
Last visit: 7/3/2012
Posts: 4
Rating:
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Thanks for useful data.
Seems to me, it's impossible to get the manufacturers winding details (number of turns per coil, wire size...).
Zlatkodo
Top
Page 1 of 1 (3 items)
Actions