Technical Forum

SINUMERIK / SIMODRIVES / MASTERDRIVES / SIMOTION / SINAMICS

Energy conservation system for plant

Thread Starter: RAJKIRAN   Started: 5/15/2012 1:14 PM   Replies: 5

« Previous thread Next thread »
Page 1 of 1 (6 items)
  5/15/2012, 1:14 PM
Joined 8/18/2009
Last visit: 4/17/2013
Posts: 464
Rating:
Rated: Outstanding [3.63 out of 5 / rated 32 time(s)]. (32) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Dear Expert,
 I want to used energy conservation system for plant by using Suitable drive...
I have all Pump/Motor's Power rating(in KW & HP),current rating & starter type of whole plant....
I want to know any extra I/P required from above list for energy conservation system.
Also tell me if there is any important doc. so that by using this doc. I can establish total energy conservation system & send energy conservation system PPT.


Rajkiran Patil

Executive Project Eng r.- Process Automation


Top
  5/16/2012, 10:12 AM
Joined 7/8/2009
Last visit: 5/17/2013
Posts: 1167
Rating:
Rated: Excellent [4.25 out of 5 / rated 326 time(s)]. (326) 
Rated: Excellent [4.25 out of 5 / rated 4 time(s)]. (4) 

RAJKIRAN wrote:
Dear Expert,

 I want to used energy conservation system for plant by using Suitable drive...

I have all Pump/Motor's Power rating(in KW & HP),current rating & starter type of whole plant....

I want to know any extra I/P required from above list for energy conservation system.

Also tell me if there is any important doc. so that by using this doc. I can establish total energy conservation system & send energy conservation system PPT.

 



Hello Rajkiran,

Energy Conservation System is really Big thing and that too if your Plant is Big

As first step, you need to study every Load which are very much cruical and have a huge part in total consumption, then you need to workout to reduce consumption for same

You need Power Rating, and application detail to select any Drive. Replacing so many DOL/SoftStarter with Drives will be result in to Heavy investment at Start so you have to Optimise between all this

Using Drive For every direct motor, will result in to Energy Saving

You can think out of using Different features of Drive for saving Energy, like use of PID in Compressor

Another thing you is constant power/load monitoring System in your Plant

Regards
Devesh




=== Edited by Vithani @ 5/16/2012 5:28 PM [GMT ] ===



Please say Thanks if your Problem is Solved.. :-)
Top
Thank you for this post from:
  5/17/2012, 7:35 AM
Joined 8/18/2009
Last visit: 4/17/2013
Posts: 464
Rating:
Rated: Outstanding [3.63 out of 5 / rated 32 time(s)]. (32) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Thanks Vithani,
could you provide any doc. regarding this so this will help me...

Rajkiran Patil

Executive Project Eng r.- Process Automation


Top
  5/17/2012, 8:43 PM
Joined 12/29/2011
Last visit: 6/7/2012
Posts: 32
Rating:
Rated: Excellent [4.25 out of 5 / rated 4 time(s)]. (4) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Here is a link to a really good writeup on Energy conservation using VSD's

http://oee.nrcan.gc.ca/industrial/equipment/variable-frequency-drives/17167


Best Regards
Mr_Al
Top
  5/25/2012, 10:03 PM
Joined 4/28/2010
Last visit: 3/8/2013
Posts: 58
Rating:
Rated: Excellent [4.56 out of 5 / rated 16 time(s)]. (16) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Dear Rajkiran,

You can use Sinasave software for estimation of energy conservation by using drives.
Please download sinasave from www.siemens.com/sinasave.

Alternatively you can use Sizer web engineering for the same purpose.
Please visit the following link.
https://www.automation.siemens.com/sizer-ld/Pages/SinaSave/StartSinaSave.aspx

These tools are excellent for estimating energy saving for different loads in an industry.

Regards
Ajay Gupta
  
Top
  6/26/2012, 3:12 PM
Joined 6/25/2012
Last visit: 6/29/2012
Posts: 5
Rating:
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
RAJKIRAN wrote:
Dear Expert,
 I want to used energy conservation system for plant by using Suitable drive...
I have all Pump/Motor's Power rating(in KW & HP),current rating & starter type of whole plant....
I want to know any extra I/P required from above list for energy conservation system.
Also tell me if there is any important doc. so that by using this doc. I can establish total energy conservation system & send energy conservation system PPT.



It really is a big thing tight now to use energy conservation for plants. I started using it for my own plants from serenata online uk and it works really great so far. I had someone coming over to explain me the whole procedure of energy conservation and he also handed me a manual for the correct utilization.
Top
Page 1 of 1 (6 items)
Actions