Technical Forum

Motion Control System SIMOTION

Not Upload project simotion D435

Thread Starter: Urantia   Started: 6/15/2012 11:24 PM   Replies: 5

« Previous thread Next thread »
Page 1 of 1 (6 items)
  6/15/2012, 11:24 PM
Joined 10/23/2009
Last visit: 3/25/2013
Posts: 67
Rating:
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 

Hi all,

Why is not possible to Upload a project in Scout (Versión 4.2)
with the option Load CPU/Drive Unit to PG.

I´m try to make the project consistent Upload the program to PG
but always the module D435 appear inconsistent. Is like
Upload does not work.

Regards.

Top
  6/16/2012, 7:27 AM
Joined 5/12/2006
Last visit: 5/26/2013
Posts: 1555
Rating:
Rated: Excellent [4.18 out of 5 / rated 115 time(s)]. (115) 
Users with special expertise supervising conferences
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Hello,

is this projekt new created with V4.2  or an older converted project?
When you go online there ist a window "Target Device Output" in the deteil view.
Can you post the messages from this window?

Regards
Christoph
Top
  6/18/2012, 11:20 PM
Joined 10/23/2009
Last visit: 3/25/2013
Posts: 67
Rating:
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 

Dear Christoph,

attached the pictures.

1.- BeforeUpload, image before upload
2.- AfterUpload, first image after upload
3.- AfterUpload2, second image after upload.

Like you see the images Before and After, (box reed) you realize that the inconsistente D435 module remain.

I suppose that the inconsistent should be disappear. I nedd that status for D435
I need consistency in my program, for to know the status of th e proggram.

Why nothing happen? and appear  the same inconsistente that before the upload.

I have the original versión for the program V4.2.1



Best  regards


Attachment: Upload.zip  (18 Downloads)

Top
  6/19/2012, 8:56 AM
Joined 5/12/2006
Last visit: 5/26/2013
Posts: 1555
Rating:
Rated: Excellent [4.18 out of 5 / rated 115 time(s)]. (115) 
Users with special expertise supervising conferences
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Hello,

in your case the HWConfig is inconsistency.
SIMOTION Upload doesn't upload any HWConfig data, only SIMOTION data ist uploaded.
So you can Download the projekt so the actual HWConfig ist downloaded or you maka a Upload of the Station in HWConfig.

Regards
Christoph
Top
  6/21/2012, 7:28 PM
Joined 10/23/2009
Last visit: 3/25/2013
Posts: 67
Rating:
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Hi CristophD,

Thanks for you help.

The solution was simple, just had to open the original project from the folder.
Previously opened the project from an compressed archive (.ZIP)
with the option  "Retrieve from archive" in 
scout 4.2.1.
That was the mistake and I don´t know why happens with the Scout
with step7 works well  the option  "Retrieve from archive".


Any comment?

Regards.
Top
  6/22/2012, 7:29 AM
Joined 5/12/2006
Last visit: 5/26/2013
Posts: 1555
Rating:
Rated: Excellent [4.18 out of 5 / rated 115 time(s)]. (115) 
Users with special expertise supervising conferences
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Hello,

"Retrieve from Archive" in scout ist exactly the same how in step7.
Scout calls the Step7 Simatic Manager function .

That should not the problem .

Regards
Christoph
Top
Page 1 of 1 (6 items)
Actions