SIMATIC WinCC
Problem activating wincc project
Thread Starter: lakebodom Started: 6/13/2012 12:26 PM Replies: 5

6/13/2012, 12:26 PM
|
Joined 6/13/2012
Last visit: 11/29/2012
Posts: 6
Rating:
(0)
|
(0)
|
Hi! I have problem while activating my wincc project . The activation stops during the activation of allarm login and runtime doesn't run. I activated graphics runtime,global script, alarm login, tag login and archive user. The version of wincc is 7.0 sp2 Update 1. No antivirus or other programs are installed on the pc, i installed only wincc. My hardware pc is: Model: Acer Aspire M1930 Rating: 220-240Vac, 3.15A, 50Hz Windows 7 Pro SP1 32 Bit CPU: Intel Core i3 Processor 2120 RAM: 4GB DDR3 memory HDD: 400 GB Hard Drive wdc wd5000aakx-001ca0 ata device OPTICAL: PIONEER DVD-RW DVR-219RS ATA DEVICE VIDEO: Nvidia GeForce 510 1024 M LAN: Integrated LAN 10/100/1000 MODEM: none KEYBOARD: USB keyboard MOUSE: USB Optical mouse SPEAKER: None BIOS: P02-A2L I enclose diagnose log file.
Thank you
=== Edited by lakebodom @ 6/13/2012 12:28 PM [GMT ] ===
=== Edited by lakebodom @ 6/13/2012 12:27 PM [GMT ] ===
|
|
|
|
|

6/13/2012, 2:23 PM
|
Joined 2/22/2006
Last visit: 5/18/2013
Posts: 202
Rating:
(19)
|
(0)
|
Hi,
Try to create new WinCC project, add Alarm Logging & Tag Logging to start up list and activate. This to check if WinCC is OK. If it so, open the problem WinCC project and try to reset Alarm Logging archives (segment) from Alarm Logging editor. Then activate the project again.
I hope that info will help you to resolve the problem.
regards smy
|
|
|
|

6/13/2012, 3:23 PM

6/14/2012, 11:42 AM
|
Joined 6/13/2012
Last visit: 11/29/2012
Posts: 6
Rating:
(0)
|
(0)
|
Good morning i have seen that wincc 7.0 sp2 is not compatible with win 7 sp1. Is there a way to downgrade win7 sp1 to win7 without sp1? The pc is new and sp1 is integrated in the cd installation of windows 7, it is not an upgrade.
Thank you
|
|
|
|

6/14/2012, 12:28 PM
|
Joined 10/11/2006
Last visit: 5/16/2013
Posts: 1741
Rating:
(77)
|
(0)
|
|
|
|
|

6/19/2012, 9:12 PM
|
Joined 6/13/2012
Last visit: 11/29/2012
Posts: 6
Rating:
(0)
|
(0)
|
|
|
|
|
Actions