SINAMICS
hardware limit switch on virtual drive
Thread Starter: looka Started: 6/12/2012 9:16 AM Replies: 0

6/12/2012, 9:16 AM
|
Joined 3/2/2012
Last visit: 11/9/2012
Posts: 1
Rating:
(0)
|
(0)
|
Hi,
I have CU320 and s120 power drives. I have 4 synchronisation (physical motor) axes, joined to one positioning (virtual) axis. I have two limit switches on each physical axis, connected to CU and configured in starter as Hardware Limit Switch for corresponding axis. So far so good, but:
How can I stop all motors, when first limit switch is hit? I would need to configure somehow also virtual axis' limit switches.
Suggested option was to set "Report error of master axis" to "Actual values", under Technology -> Axes -> <my axis> -> Monitoring -> tab Synchronous operation. This does not work.
I figured out a way, to connect same signals to External Alarm 1,2 and 3 to my CU, but this way kills possibility to move away from hit limit switch.
I am using techonogy version 4.1.1, so sfb 480 and further are out of question. Thanks
=== Edited by looka @ 6/12/2012 12:40 PM [GMT ] === added tech version
|
|
|
|
|
Actions