Technical Forum

Communication / Networks

connect 3 ABB drives ACS550 to an Profibus Master in S7-1200

Thread Starter: Bepke   Started: 6/4/2012 7:15 AM   Replies: 2

« Previous thread Next thread »
Page 1 of 1 (3 items)
  6/4/2012, 7:15 AM
Joined 10/22/2010
Last visit: 11/18/2012
Posts: 6
Rating:
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Hello,
I also need to connect 3 ABB drives ACS550 to an Profibus Master in S7-1200.
While there is no SFC14/15 in S7-1200, does someone has an example to do this ?
Thanks and beste regards.



=== Edited by O_Moderator @ 6/6/2012 11:26 AM [GMT ] ===
new subject after splitting from Profibus connection ABB drive on S71200

Top
  6/11/2012, 9:17 AM
Joined 6/17/2011
Last visit: 5/23/2013
Posts: 1283
Rating:
Rated: Excellent [4.05 out of 5 / rated 81 time(s)]. (81) 
Users with special expertise supervising conferences
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Hello Bebke,

this is not exactly what you are looking for but maybe this example can already help you further:

http://support.automation.siemens.com/WW/view/en/56749384

This example is about using CM 1243-5 as Profibus master with Sinamics as slave.

Maybe you will also find som einformation in the system manual:

http://support.automation.siemens.com/WW/view/en/36932465

Gruß / best regards
Rated X
Top
  6/11/2012, 12:16 PM
Joined 11/25/2011
Last visit: 5/20/2013
Posts: 30
Rating:
Rated: Outstanding [3.75 out of 5 / rated 4 time(s)]. (4) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Hi.Hear is a project with ACS355 drives.But its running also with ACS550

Attachment: TTL_STEAMS_LINE - Copy.zip  (79 Downloads)



=== Edited by O_Moderator @ 6/11/2012 1:58 PM [GMT ] ===



Top
Page 1 of 1 (3 items)
Actions