Technical Forum

Process Control Systems SIMATIC PCS 7

parameter assignment error preventing start up

Thread Starter: chitturi   Started: 6/2/2012 4:56 PM   Replies: 2

« Previous thread Next thread »
Page 1 of 1 (3 items)
  6/2/2012, 4:56 PM
Joined 7/21/2008
Last visit: 5/16/2013
Posts: 10
Rating:
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Dear All,

Can any body let me know the solution for the below mentioned probelm.

PCS7 V7.0 SP1 with hardware 417-4ht14 firmware v4.5.5 redundant system. 
while configuring hardware i had used the 417-4ht14 ,v4.5 After downloading the programme,  CPU is not going to run mode.
attached the diagnostic buffer.

Is above hardware will support PCS7 V7.0 SP1 or any updates required.

regards,
chitturi

Attachment: New Bitmap Image.JPG  (21 Downloads)

Top
  6/6/2012, 10:53 AM
Joined 2/24/2011
Last visit: 5/22/2013
Posts: 676
Rating:
Rated: Excellent [4.45 out of 5 / rated 58 time(s)]. (58) 
Users with special expertise supervising conferences
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 

Has this CPU been in the catalog of HW config dialog?

Top
  6/7/2012, 8:12 AM
Joined 6/12/2009
Last visit: 9/14/2012
Posts: 288
Rating:
Rated: Outstanding [3.87 out of 5 / rated 15 time(s)]. (15) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
chitturi wrote:
Dear All,

Can any body let me know the solution for the below mentioned probelm.

PCS7 V7.0 SP1 with hardware 417-4ht14 firmware v4.5.5 redundant system. 
while configuring hardware i had used the 417-4ht14 ,v4.5 After downloading the programme,  CPU is not going to run mode.
attached the diagnostic buffer.

Is above hardware will support PCS7 V7.0 SP1 or any updates required.

regards,
chitturi



Best try and get the latest HSP from this site for PCS7 V7.0. Then your hardware catalog will have all the latest released modules for your PCS7 version. try replacing the existing CPU's with the proper firmware version .

IMPOSSIBLE SPELLS I'M POSSIBLE
Top
Page 1 of 1 (3 items)
Actions