Technical Forum

Process Control Systems SIMATIC PCS 7

S7 F System

Thread Starter: likevc   Started: 5/31/2012 2:48 PM   Replies: 10

« Previous thread Next thread »
12» Page 1 of 2 (11 items)
  5/31/2012, 2:48 PM
Joined 11/24/2011
Last visit: 8/7/2012
Posts: 15
Rating:
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
I am a beginner ,when i download my programmer ,it appear errors .
why? the menmery card do not include any saftey blocks. I can see it when I  online. 

Attachment: ERROR.jpg  (36 Downloads)

Top
  5/31/2012, 2:53 PM
Joined 11/24/2011
Last visit: 8/7/2012
Posts: 15
Rating:
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
 programmer  password :likevc
attachment is my programmer.

Attachment: Demo.zip  (9 Downloads)

Top
  5/31/2012, 3:29 PM
Joined 4/19/2008
Last visit: 5/11/2013
Posts: 1261
Rating:
Rated: Outstanding [3.96 out of 5 / rated 113 time(s)]. (113) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
likevc wrote:
I am a beginner ,when i download my programmer ,it appear errors .
why? the menmery card do not include any saftey blocks. I can see it when I  online. 


Hello likevc,

Can you tell me which Version of the Step 7 & F system you have ?astonished

its Important during opening of the backup....which you post...blink

Ammy

New for every one..............

“No duty is more urgent than that of returning thanks.”
If Problem Solved......!

Top
  6/1/2012, 2:58 AM
Joined 11/24/2011
Last visit: 8/7/2012
Posts: 15
Rating:
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Step 7 v5.5SP2 +F system V 6.0
Top
  6/1/2012, 8:29 AM
Joined 4/19/2008
Last visit: 5/11/2013
Posts: 1261
Rating:
Rated: Outstanding [3.96 out of 5 / rated 113 time(s)]. (113) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
likevc wrote:
Step 7 v5.5SP2 +F system V 6.0


Hello likevc,

As I have F System V6.1 SP1 with CFC V8.0 I don't find any problem During Downloading with PLCSIM,

I can tell you Please Update to
F System V6.1 SP1 & then try......

& one more in your project I have seen
6ES7326-1BK00-0AB0 Module, this Module is no longer available Please Replace with 6ES7326-1BK02-0AB0 then try.......blink

If you are not working on actual Hardware....astonished

Ammy

New for every one..............

“No duty is more urgent than that of returning thanks.”
If Problem Solved......!

Top
  6/2/2012, 2:16 AM
Joined 11/24/2011
Last visit: 8/7/2012
Posts: 15
Rating:
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Yes,if you download it to PLCSIM ,it's OK. But if you download to a really  CPU with a Flash card ,It would be appear the errors.
   I had asked Siemens technology support via tel 400,they told me that it must be downloaded  by  way of  a cardreader for the first time  if you use a flash card. If you use a RAM card ,it would be good.
   But I have no cardreader and RAM card ,what can I do? It is not helpful  by means of   PLC-> DOWNLOAD  TO MEMORY CARD
Top
  6/4/2012, 11:18 AM
Joined 11/24/2011
Last visit: 8/7/2012
Posts: 15
Rating:
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 

Who can give me an answer?

Top
  6/4/2012, 1:44 PM
Joined 7/20/2010
Last visit: 3/25/2013
Posts: 11
Rating:
Rated: Excellent [5 out of 5 / rated 1 time(s)]. (1) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Hello likevc,

Did you switch the CPU to stop? you can only change the safety program with either safety mode deactivated or when in stop mode. When you download from charts you will be prompted for this, but i'm not sure you get this when transferring directley to memory card.
 
Did you allso check your setting in the hardware configuration that the CPU is to be used as a safety CPU? you have to enable this setting yourself and enter a password for the safety program.    



=== Edited by CK84 @ 6/4/2012 1:45 PM [GMT ] ===


Top
  6/5/2012, 1:57 PM
Joined 11/24/2011
Last visit: 8/7/2012
Posts: 15
Rating:
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
I had set CPU  in stop modle.the  problem  is i can not download to CPU
 with  a lash card.

Attachment: ERROR.jpg  (7 Downloads)

Top
  6/6/2012, 8:44 AM
Joined 7/20/2010
Last visit: 3/25/2013
Posts: 11
Rating:
Rated: Excellent [5 out of 5 / rated 1 time(s)]. (1) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
likevc,

Did you try the "download program to memory card" funtion?

you won't be able to download your program to a flash card from the charts.

Select you block folder and go to PLC>download program to memory card.
This will download the blocks directly to the flash card.

Attachment: Download_flashcard.JPG  (10 Downloads)

Top
12» Page 1 of 2 (11 items)
Actions