Technical Forum

Motion Control System SIMOTION

External Encoder Motion State Position Tag

Thread Starter: albertorivas   Started: 3/25/2009 6:31 PM   Replies: 4

« Previous thread Next thread »
Page 1 of 1 (5 items)
  3/25/2009, 6:31 PM
Joined 3/13/2009
Last visit: 2/28/2010
Posts: 7
Rating:
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
How do I refer to the Tag from the "External Encoder Motion State Position" in the expert list, in order to use it my Ladder and MCC programs.

Thank you
Top
  3/26/2009, 7:46 AM
Joined 5/12/2006
Last visit: 5/19/2013
Posts: 1546
Rating:
Rated: Excellent [4.18 out of 5 / rated 115 time(s)]. (115) 
Users with special expertise supervising conferences
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Hello,

you can get the variable via <name of encoder>.motionstate.position.

When you have open the ladder/mcc program you can access the symbolbrowser of the TO encoder and drag and drop the variable directly to the ladder/program.

Regards
Christoph
Top
  4/20/2009, 2:47 PM
Joined 11/6/2008
Last visit: 5/20/2009
Posts: 8
Rating:
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 

How can this be done in ST?

I use

myCTRL_dataPid.numericActValue   :=  Myencoder.motionstate.position;

(I have also used D425.myencoder.motionstate.position)

When I try to compile my program I get an error:


Error ST_pidcontrol: 10014 :Already specified technology packages do not support the type of TO "Myencoder"
Error ST_pidcontrol(84) : 6003 :Variable ID expected hoekencoder
Error Error on:
Error Syntax error (ret = 0xbe03000b)

can anyone help me? Thanks in advance!!

Jonas




=== Edited by jonasddd @ 4/20/2009 2:48 PM [GMT ] ===


=== Edited by jonasddd @ 4/20/2009 2:48 PM [GMT ] ===


Top
  4/21/2009, 5:32 AM
Joined 5/12/2006
Last visit: 5/19/2013
Posts: 1546
Rating:
Rated: Excellent [4.18 out of 5 / rated 115 time(s)]. (115) 
Users with special expertise supervising conferences
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Hello,

which Technology Packages are mapped on the cpu?
Have you use this packages in the ST program (f.e. USEPACKAGE CAM ?)

Regards
Christoph
Top
  5/25/2012, 9:12 AM
Joined 3/2/2007
Last visit: 5/17/2013
Posts: 150
Rating:
Rated: Outstanding [4 out of 5 / rated 1 time(s)]. (1) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
kindly, how did you solve these two errors 10014 and 6003 ? thank you
Top
Page 1 of 1 (5 items)
Actions