Technical Forum

Programming Devices

PG M Screen repair

Thread Starter: GrantForeman   Started: 5/21/2012 2:06 PM   Replies: 5

« Previous thread Next thread »
Page 1 of 1 (6 items)
  5/21/2012, 2:06 PM
Joined 5/18/2012
Last visit: 11/22/2012
Posts: 12
Rating:
Rated: Excellent [5 out of 5 / rated 1 time(s)]. (1) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 

Hey guys,

Does anyone have experience removing the cover off the screen, this won't come off.
I'm afraid to break it, where I circled in the attachment is where it is still attached and I cant see inside to see what is holding it.

The screen keeps flashing/going crazy, and it is solved with a good slap, but I don't think this is the best solution, so I need to get inside and make sure the connections are not loose.

It is a Simatic PG M


Attachment: simatic pg.JPG  (28 Downloads)

Top
  5/21/2012, 4:21 PM
Joined 9/7/2007
Last visit: 5/15/2013
Posts: 292
Rating:
Rated: Outstanding [3.44 out of 5 / rated 32 time(s)]. (32) 
Rated: Excellent [5 out of 5 / rated 1 time(s)]. (1) 
GrantForeman wrote:

Hey guys,

Does anyone have experience removing the cover off the screen, this won't come off.
I'm afraid to break it, where I circled in the attachment is where it is still attached and I cant see inside to see what is holding it.

The screen keeps flashing/going crazy, and it is solved with a good slap, but I don't think this is the best solution, so I need to get inside and make sure the connections are not loose.

It is a Simatic PG M


Does this happened after an accident or some liquids spilled inside?


Best Regards
Top
Thank you for this post from:
  5/21/2012, 7:52 PM
Joined 9/27/2005
Last visit: 6/17/2013
Posts: 944
Rating:
Rated: Above avarage [2.61 out of 5 / rated 36 time(s)]. (36) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
I think that there is no serious efforts shall be applied. as alternative can take the LCD monitor (15") and attach it to the back of the cover of Field pg. By Field Pg monitor can be connected either VGA-cable, or through a converter USB-DVI/HDMI.
Top
Thank you for this post from:
  5/23/2012, 1:24 PM
Joined 5/18/2012
Last visit: 11/22/2012
Posts: 12
Rating:
Rated: Excellent [5 out of 5 / rated 1 time(s)]. (1) 
Rated: Excellent [5 out of 5 / rated 1 time(s)]. (1) 
In the end, I had to be a little more brutal, and fortunately, the little plastic clip did not break, it was just awkward.

I literally only touched the flexi-strip connected to the to the LCD panel, and the screen displayed correctly, so I just made sure the connection was good and re-secured the sticky tape.

No, there was no coffee/liquid spilt inside (At least not on this laptop) Rnf:lblSmileyTooltip_

Gre_m, seriously???
The point of having a FIELD PG is that you don't need to wheel your desk up a ladder and onto the gantry of a machine in order to use a laptop. astonished

Thanks anyway, Grant
Top
Thank you for this post from:
  5/23/2012, 2:22 PM
Joined 3/15/2008
Last visit: 6/18/2013
Posts: 4456
Rating:
Rated: Outstanding [3.89 out of 5 / rated 415 time(s)]. (415) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
GrantForeman wrote:
...
Gre_m, seriously???
The point of having a FIELD PG is that you don't need to wheel your desk up a ladder and onto the gantry of a machine in order to use a laptop. astonished




Rnf:lblSmileyTooltip_ Rnf:lblSmileyTooltip_ Rnf:lblSmileyTooltip_

Industrieautomation: Softwareerstellung und Inbetriebnahme weltweit.
http://www.ibn-service.com
Top
  6/25/2012, 2:10 PM
Joined 6/25/2012
Last visit: 6/29/2012
Posts: 5
Rating:
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
I think that you should really have someone take a look at it rather than go on the solution to handle everything coming from your end.  And from the look of things, there are quite a number of other choices to go with just to name a few.

But with the other options being consumed, you should be seeing no problem with how they are going to be solved just like that
Top
Page 1 of 1 (6 items)
Actions