Technical Forum

Process Instrumentation / Analytics / Weighing Systems SIWAREX

IM153-4 and Siwarex U

Thread Starter: protivogas   Started: 5/8/2012 6:26 PM   Replies: 4

« Previous thread Next thread »
Page 1 of 1 (5 items)
  5/8/2012, 6:26 PM
Joined 3/14/2009
Last visit: 5/20/2013
Posts: 9
Rating:
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Found the following problem... IM153-4(PN) with 5 Siwarex modules when power off and then power on stand on SF... the module doesn't see. Restart of the processor module doesn't help... only removal and repeated installation of the module from the tire eliminates SF
In the similar project the same only with one Siwarex module after inclusion the mistake doesn't arise and everything remarkably works.
Top
  5/8/2012, 7:30 PM
Joined 1/3/2006
Last visit: 6/18/2013
Posts: 549
Rating:
Rated: Outstanding [3.83 out of 5 / rated 29 time(s)]. (29) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
What does Module Information says?
Top
  5/9/2012, 9:49 AM
Joined 8/20/2009
Last visit: 6/2/2013
Posts: 69
Rating:
Rated: Above avarage [3 out of 5 / rated 4 time(s)]. (4) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Dear,

After power up, pls check if the program blocks are available in the CPU. Also, check whether after power recycle online program is matching with the your backup program. May be program in flash card is different.

Check also that the Scale and Vector DB does not initialize on power up.

Rnf:lblSmileyTooltip_ Vishp.
Top
  5/9/2012, 12:24 PM
Joined 3/14/2009
Last visit: 5/20/2013
Posts: 9
Rating:
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 

missing module in slot 1,2,3,4,5,6,7,8

Top
  5/9/2012, 12:28 PM
Joined 3/14/2009
Last visit: 5/20/2013
Posts: 9
Rating:
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
VishP wrote:
Dear,

After power up, pls check if the program blocks are available in the CPU. Also, check whether after power recycle online program is matching with the your backup program. May be program in flash card is different.

Check also that the Scale and Vector DB does not initialize on power up.

Rnf:lblSmileyTooltip_ Vishp.


I have no problems with program start... other 7 racks with IM153-4 are normally initialized and work... and two racks work through WDS on a wireless network and from them power is periodically removed... so after power restorating they are synchronized and work... the unique rack with which is a problem it is that where weight modules are established

Attachment: HW.jpg  (4 Downloads)



=== Edited by protivogas @ 5/9/2012 12:41 PM [GMT ] ===


=== Edited by protivogas @ 5/9/2012 12:29 PM [GMT ] ===



Top
Page 1 of 1 (5 items)
Actions