Technical Forum

Programming Devices

Upgrade for Field PG M2

Thread Starter: machaeis   Started: 3/29/2012 10:32 PM   Replies: 7

« Previous thread Next thread »
Page 1 of 1 (8 items)
  3/29/2012, 10:32 PM
Joined 12/8/2011
Last visit: 4/4/2013
Posts: 3
Rating:
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Hello .. I'm upgrading a Field PG M2, and I would like to know how do not to have conflict of software. I need to use the softwares: WinCC2008, TIA V11, STEP7 V5.5, MicroWin 4.0 SP9, SETP 5 V7.2, Protool SP3+HF3, Drive ES V5.5, Profibus Config V5.1, V7.3 HMI Advanced.
 I intend to use three partitions: Windows 7, Windows XP for SETP 5 Operations and old softwares and other Windows XP only for Sinumerik softwares (802, 810, 840D tool boxes).



=== Edited by machaeis @ 3/29/2012 10:35 PM [GMT ] ===


Top
  4/3/2012, 7:37 AM
Joined 12/1/2009
Last visit: 5/18/2013
Posts: 322
Rating:
Rated: Outstanding [3.57 out of 5 / rated 28 time(s)]. (28) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
machaeis wrote:
Hello .. I'm upgrading a Field PG M2, and I would like to know how do not to have conflict of software. I need to use the softwares: WinCC2008, TIA V11, STEP7 V5.5, MicroWin 4.0 SP9, SETP 5 V7.2, Protool SP3+HF3, Drive ES V5.5, Profibus Config V5.1, V7.3 HMI Advanced.
 I intend to use three partitions: Windows 7, Windows XP for SETP 5 Operations and old softwares and other Windows XP only for Sinumerik softwares (802, 810, 840D tool boxes).


Hi,

I would make two partitions: Windows XP first with all software packages except the TIA.
On second partition Win7 and the TIA only.
I dont see the need of having a third partition with Win XP.

It's all up to you!

Regards.


  

-------------------------------------------------------------------------------------------------------
Give us your feedback and show us your respect!
We take our free time to support you with our knowledge and experience.
If this post is helpfull to you kindly click on "Rate" or "Thank".
Top
Thank you for this post from:
  4/20/2012, 3:47 PM
Joined 9/27/2005
Last visit: 5/8/2013
Posts: 934
Rating:
Rated: Above avarage [2.61 out of 5 / rated 36 time(s)]. (36) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
You can also use virtual machine such a virtual box, wmvare. With windows7 you can use xp mode
Top
  4/20/2012, 4:29 PM
Joined 3/15/2008
Last visit: 5/18/2013
Posts: 4434
Rating:
Rated: Outstanding [3.88 out of 5 / rated 409 time(s)]. (409) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
gre_m wrote:
You can also use virtual machine such a virtual box, wmvare. With windows7 you can use xp mode


If you like to use S5 Online on VM - machine, first make shure, that seriall port is supported or your USB - adapter is supported!

Industrieautomation: Softwareerstellung und Inbetriebnahme weltweit.
http://www.ibn-service.com
Top
  4/21/2012, 8:57 AM
Joined 9/27/2005
Last visit: 5/8/2013
Posts: 934
Rating:
Rated: Above avarage [2.61 out of 5 / rated 36 time(s)]. (36) 
Rated: Very Good [2 out of 5 / rated 1 time(s)]. (1) 
for s5 need S5 EPROM adapter. As variant it can work without wirtual. Other soft as may be install on virtual. But i prefer  separate partition
Top
  4/26/2012, 11:15 PM
Joined 12/8/2011
Last visit: 4/4/2013
Posts: 3
Rating:
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 

OK...
        I used one little of each, and I mounted a new hard disk with five partitions:

First Partition (100GB) - Windows Seven: for new Simatic softwares

Second Partition (100GB) - Windows XP: for old simatic softwares, and others that I use, also with Virtual PC with MS-DOS 6.22 for IBS and PCIN 4.2 Softwares. ( I did one cpu to Step 5 too).

Third Partition (20GB) - Windows XP only to Sinumerik operations (HMI Advanced for example).

Fourth Partition (180GB) - Data Partition.

Fifth Partition (100GB) -  Recovery Partition (backup).

To this moment I tested all softwares and all right with all..

Thanks guys!

Top
  4/27/2012, 6:16 AM
Joined 3/15/2008
Last visit: 5/18/2013
Posts: 4434
Rating:
Rated: Outstanding [3.88 out of 5 / rated 409 time(s)]. (409) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
machaeis wrote:

OK...
        I used one little of each, and I mounted a new hard disk with five partitions:
...



Which Partition Manager do you use?


Industrieautomation: Softwareerstellung und Inbetriebnahme weltweit.
http://www.ibn-service.com
Top
  4/27/2012, 9:10 PM
Joined 12/8/2011
Last visit: 4/4/2013
Posts: 3
Rating:
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 

I have not used OS Manager software, but guess that I would use Acronis OS Selector!

I created all the partitions in the installation of Windows Seven. First I installed all the systems (win7 + winxp1 + winxp2). After I installed Acronis True Image software on Windows Seven and activated the Recovery Manager Startp. Then the system reboots I made a backup of each important point for security.
Everything worked normal ... I have two menus, the boot system Windows 7, and after XP menu.

Top
Page 1 of 1 (8 items)
Actions