Technical Forum

Visualization

Press and hold increment jog method

Thread Starter: ahsan1820   Started: 4/14/2012 1:26 PM   Replies: 6

« Previous thread Next thread »
Page 1 of 1 (7 items)
  4/14/2012, 1:26 PM
Joined 6/7/2011
Last visit: 5/17/2013
Posts: 112
Rating:
Rated: Above avarage [3 out of 5 / rated 1 time(s)]. (1) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
please tell me how to make a push button which continuously increases/decrease the value of a vriable in PLC .
Top
  4/14/2012, 4:06 PM
Joined 3/21/2006
Last visit: 5/14/2013
Posts: 9063
Rating:
Rated: Outstanding [3.78 out of 5 / rated 820 time(s)]. (820) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Hello,

Please, specify what software will be used there? Basically in WinCC or WinCC Flex have in built buttons for increase/decrease. Just need to assign them to a specific tag which is connceted in PLC logic to do the job.

Best regards,
Hristo Mihalev
Top
  5/14/2012, 5:19 AM
Joined 7/25/2009
Last visit: 5/18/2013
Posts: 398
Rating:
Rated: Very Good [1.5 out of 5 / rated 4 time(s)]. (4) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
ahsan1820 wrote:
please tell me how to make a push button which continuously increases/decrease the value of a vriable in PLC .


Hello ahsan1820
can you give the more detail what you are going to devlop your logic..

regards

algudkar

regards
Algudkar sh..

Top
  5/14/2012, 2:41 PM
Joined 5/28/2009
Last visit: 11/29/2012
Posts: 118
Rating:
Rated: Outstanding [3.56 out of 5 / rated 9 time(s)]. (9) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
ahsan1820 wrote:
please tell me how to make a push button which continuously increases/decrease the value of a vriable in PLC .


Dear ahsan1820

It is hardware pushbutton or soft button in HMI please mention it.

Regards,
SkD
Top
  5/16/2012, 9:58 AM
Joined 10/28/2009
Last visit: 2/13/2013
Posts: 103
Rating:
Rated: Outstanding [3.17 out of 5 / rated 6 time(s)]. (6) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
hi,

please elaborate your requirement, with following details,

1. software used: WinCC or WinCC Flex
2. Exact requirement why you need this type of pushbutton
3. do you want the soft or the hard wired button

also think from the entire application perspective and give the details accordingly.

Rnf:lblSmileyTooltip_

Regards,
PPND
Top
  5/30/2012, 8:15 AM
Joined 2/22/2011
Last visit: 5/18/2013
Posts: 90
Rating:
Rated: Excellent [4.5 out of 5 / rated 2 time(s)]. (2) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
ahsan1820 wrote:
please tell me how to make a push button which continuously increases/decrease the value of a vriable in PLC .



Dear  ahsan

          Make a logic in the plc program that when the push button(hold button) is actuated
then make the timer on/of ,on/off followed by an up counter then ur value will add deponding on the pulse on/off, on/off the timer

when u press the decerese button v make the down counter act and the value will get decrese

u can move the counter value to your  desired out put
Rnf:lblSmileyTooltip_

Thanks regards
ANBUGEETHAN GOWDA
Top
  2/7/2013, 8:16 AM
Joined 9/14/2011
Last visit: 4/9/2013
Posts: 120
Rating:
Rated: Good [1 out of 5 / rated 1 time(s)]. (1) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Hi ,

If u are using a seperate Push Buttons for Inc & Decreasing this can be done in the button properties itself.

Set a bit while press & reset the same bit while release so that u can use these respective bits in the PLC logic..

Hope it helps

Regards,

Nelliyan.G
Top
Page 1 of 1 (7 items)
Actions