Technical Forum

SIMATIC 505

Comunication between HMI MP277 and TI 535 1212

Thread Starter: ern_z   Started: 11/15/2011 11:17 AM   Replies: 0

« Previous thread Next thread »
Page 1 of 1 (1 items)
  11/15/2011, 11:17 AM
Joined 4/6/2007
Last visit: 4/15/2013
Posts: 3
Rating:
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
I have a HMI panel MP277 10 inch touch that must comunicate with a Texas PLC Ti 534 1212. by means of the RS 422 serial port.
I have made a very simple sample program with just one variable and with the system message window.
The comutication keeps crashing and the HMI system messages 22006 and 22007 alternatly appear.
I have tried changing all the RS422 settings in WINCC, also the byterate. I have also tried changing the RS422 cable, all with the same results. I must precise that the RS422 cable is only about 1 mt long.
I'm using WINCC SP2 Upd13 and I've load B 1.1.3.13 firmware on the MP277.

Thanks in advance
Top
Page 1 of 1 (1 items)
Actions