Technical Forum

LOGO!

Drive synchronisation

Erstellt von PISCEAN 2010 am 29.07.2012 07:43 (1 Antworten)

« Vorheriges Thema Nächstes Thema »
Seite 1 von 1 (2 Objekte)
  29.07.2012, 07:43
Beigetreten am: 23.04.2010
Letzter Besuch: 19.05.2013
Beiträge: 1148
Bewertung:
Bewertung: Herausragend [3,17 von 5 / 53 mal bewertet]. (53) 
Bewertung: keine [0 von 5 / 0 mal bewertet]. (0) 
7/29/2012, 6:56 AM
Joined 7/14/2012
Last visit: 7/17/2012
Posts: 1
Rating: Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Hi,
I have one query regarding the logo plc
I have to synchronize two drive of overhead conveyor which is 500 meter long.For synchronization i wil send the same  analog voltage for both drives.but for error detection two proximity sensors are mounted on sproket of 2 drive.so i have to count that pulses for the confirmation that both drives are synchronized & chain is not broken.

The speeds variation are 5 speed through switch.
 

Tell me and I will forget. Show me and I will remember. Involve me and I will understand. -Confucius
Top
  31.07.2012, 17:50
Beigetreten am: 19.06.2010
Letzter Besuch: 19.05.2013
Beiträge: 174
Bewertung:
Bewertung: Herausragend [3,95 von 5 / 22 mal bewertet]. (22) 
Bewertung: keine [0 von 5 / 0 mal bewertet]. (0) 
Hi PISCEAN 2010,
It seems interesting question. Please clrify me the following inorder to suggest my ideas.

Does the two motrors will drive one conveyer belt ?

Regards,
 

You like it? Rate it !


ለማንኛውም የፋብሪካ አውቶሜሽ ስራ፣ በተለይም፡

ፒ. ኤል.ሲ፣ድራይቭ፣ኮምፒዩተራይዝድ ማሽን ስራ፡በዚህ ይደውሉ 0922 493737
Top
Seite 1 von 1 (2 Objekte)
Aktionen