Technical Forum

SIMOVERT MASTERDRIVES

Masterdrive MC alarm A141

Erstellt von mariusd am 14.06.2012 14:16 (1 Antworten)

« Vorheriges Thema Nächstes Thema »
Seite 1 von 1 (2 Objekte)
  14.06.2012, 14:16
Beigetreten am: 14.06.2012
Letzter Besuch: 05.07.2012
Beiträge: 1
Bewertung:
Bewertung: keine [0 von 5 / 0 mal bewertet]. (0) 
Bewertung: keine [0 von 5 / 0 mal bewertet]. (0) 
Hi,
In one of  my MASTERDRIVE MC I ahve all the time when I try to run the motor the alarm A141. The motor is not moving.
The drive type is 6SE7018-OEP70-ZF01 and the motor type is 1FT6064-1AF71-3EG1.
Can somebody help me to identify the cause of this alarm. But please not the comments from the Manual, because these didn't help me.
Thanks
Top
  14.06.2012, 19:16
Beigetreten am: 04.06.2008
Letzter Besuch: 15.05.2013
Beiträge: 770
Bewertung:
Bewertung: Exzellent [4,39 von 5 / 225 mal bewertet]. (225) 
Benutzer mit speziellen Fachkenntnissen, die einzelne Konferenzen betreuen
Bewertung: keine [0 von 5 / 0 mal bewertet]. (0) 
mariusd wrote:
Hi,
In one of  my MASTERDRIVE MC I ahve all the time when I try to run the motor the alarm A141. The motor is not moving.
The drive type is 6SE7018-OEP70-ZF01 and the motor type is 1FT6064-1AF71-3EG1.
Can somebody help me to identify the cause of this alarm. But please not the comments from the Manual, because these didn't help me.
Thanks

Why did the MC Manual comments for Alarm A141 not help you?

Can you use the trace tool to see the position setpoint and the position actual?
Does any fault occur after the alarm?

With the drive disabled (for your safety), can you spin the motor by hand?
You could try monitoring parameter r002 for the actual speed if the encoder is working correctly, but you may also see an A140 alarm.
Regards,
Graeme

There are 10 types of people . . .
Those who understand Binary, and those who don't.
Top
Seite 1 von 1 (2 Objekte)
Aktionen