Technical Forum

SIMODRIVE Converter system

Traverse blocks in Axes 2 Not Updating

Erstellt von SteveOwen am 05.06.2012 18:12 (1 Antworten)

« Vorheriges Thema Nächstes Thema »
Seite 1 von 1 (2 Objekte)
  05.06.2012, 18:12
Beigetreten am: 05.06.2012
Letzter Besuch: 08.02.2013
Beiträge: 2
Bewertung:
Bewertung: keine [0 von 5 / 0 mal bewertet]. (0) 
Bewertung: keine [0 von 5 / 0 mal bewertet]. (0) 
Hi,
My first post so please go easy =D

I have a 2 Axis 611u simodrive positioning application but i cannot transfer the traversing blocks necessary to axis 2. I used the example software in the 611 toolbox but for some reason I cannot get the traverse information into the traverse table in drive 2.

The addresses are correct and control is fine, I just cannot move single parameters. When I trigger a write I have no busy signal and no done signal afterwards. To adjust traverse positions I must use SimoComU.

Maybe some guidance on where I might start to fault find would be nice. Everything seems good and profibus comms to drive 2 are working. just the single traverse parameters do not transfer. Drive 1 works perfectly.

Thanks.
Steve
Top
  07.06.2012, 15:02
Beigetreten am: 05.06.2012
Letzter Besuch: 08.02.2013
Beiträge: 2
Bewertung:
Bewertung: keine [0 von 5 / 0 mal bewertet]. (0) 
Bewertung: keine [0 von 5 / 0 mal bewertet]. (0) 
Bump

Does anyone have any guidance on this?
i will post some images from the software to show exactly whats going on.

If someone can help but requires more information please let me know.

As far as I can see everything is configured correctly.

Regards,

Steve
Top
Seite 1 von 1 (2 Objekte)
Aktionen