Technical Forum

SIMATIC TDC, FM458, T400

T400 download with DUST1

Erstellt von SDavies am 11.03.2008 21:57 (2 Antworten)

« Vorheriges Thema Nächstes Thema »
Seite 1 von 1 (3 Objekte)
  11.03.2008, 21:57
Beigetreten am: 11.03.2008
Letzter Besuch: 06.10.2009
Beiträge: 2
Bewertung:
Bewertung: keine [0 von 5 / 0 mal bewertet]. (0) 
Bewertung: keine [0 von 5 / 0 mal bewertet]. (0) 
I recently have been trying to connect to a T400 via DUST1, and have run into an issue where Add/Remove within PG/PC interface does not successfully install DUST1.

When I select DUST1 on the left hand side and click install the right hand side flickers and refreshes, but does not actually add DUST1.

So far i have tried to install this DUST1 on 8 different computers. 6 were using 5.4SP3, and DUST1 would not install. The other 2 were using 5.4SP1 and 5.4 SP2 and DUST1 installed fine. I'm unsure is it is the version of Simatic Manager that would cause this issue, but it seems to be a big coincident.

Can anyone provide information on how to successfully install the DUST1 protocol?

Thanks,
-Sandy
Top
  12.03.2008, 15:28
Beigetreten am: 31.08.2005
Letzter Besuch: 19.06.2013
Beiträge: 997
Bewertung:
Bewertung: Herausragend [3,85 von 5 / 122 mal bewertet]. (122) 
Benutzer mit speziellen Fachkenntnissen, die einzelne Konferenzen betreuen
Bewertung: keine [0 von 5 / 0 mal bewertet]. (0) 
Hallo Sandy,

If you have STEP7 V5.4 SP3 with D7-SYS V6.2 you have to do the following steps:

- make shure you have installed the SP3 for D7-SYS V6.2 ( download )
- contact the Hotline and ask for the hotfix that fixes your problem (I think it's hotfix2)


mfG / Best Regards

Dirk
Top
  23.01.2012, 13:38
Beigetreten am: 22.01.2012
Letzter Besuch: 23.01.2012
Beiträge: 1
Bewertung:
Bewertung: keine [0 von 5 / 0 mal bewertet]. (0) 
Bewertung: keine [0 von 5 / 0 mal bewertet]. (0) 
Sdavies

the only solution that have worked for me so far, it is the following (always works):

-Unistall all PCS7 packages

-Install the PCS7 V7.0 (Now, this is the PCS7 that actaully acepts the dust protocol)

-Install Drive ES (Wich enables the Dust Protocol), or any other soft you may have that also has this protocol;

-Now, in the Simatic Manager, Open the Set PG/PC Intaface and Add the Dust Protocol (It will be added, don´t worry)

-Upgrade you PCS7 to the latest version you wish to use.

There you go, Dust1 Protocol in a newer PCS7 version.

Haven´t erver tried the solution mentioned above, if it works, it is WAY BETTER then this one. But this one I can asure that really works.



=== Edited by Marcel Cukier @ 1/23/2012 1:38 PM [GMT ] ===


Top
Seite 1 von 1 (3 Objekte)
Aktionen