Technical Forum

ROBICON Perfect Harmony - Medium voltage converters

Robicon ID-PWM 454 GT Series HELP!

Thread Starter: NH3 Bob   Started: 5/17/2012 4:20 PM   Replies: 0

« Previous thread Next thread »
Page 1 of 1 (1 items)
  5/17/2012, 4:20 PM
Joined 5/17/2012
Last visit: 5/18/2012
Posts: 1
Rating:
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 

I have a problem with the AREF INPUTS on the old 454 GT Drive. I have been over the settings a thousand times in the menu'smad, but the Analog inputs are being held at 11ma. No change with simulator, Pressure TX, EVEN when no input is hooked up at all!Rnf:lblSmileyTooltip_  think 
As a result the VFD runs at one speed in Auto. I can speed up and slow down the VFD in manual however. I am useing a 4-20ma singnal from a PT to control the VFD Speed. REAL SIMPLE (or it should be) Are the VFD inputs toast? Or am I missing something?cry



Top
Page 1 of 1 (1 items)
Actions